I've tried several attempts to create a job desciptor for a Job Ring that would create 8 bytes of random data (via the RNG algorithm) and move it to system RAM. I keep getting errors.
Attempt #1
-----------------
header B0800005
Seq Out PTR F8000008
RAM Addr 05008000
RNG Alg 82500000
MOVE 6A220008
Resulting Status Word (JD + Status)
------------------------------
50004000 --that's where I put the JD and the intput ring was pointing there ok
4000040B -- Somethings wrong with the RNG command?
Also the SSTA is a 00000401
Attempt #2
See attached file
Original Attachment has been moved to: jd_rng_notes.txt.zip
已解决! 转到解答。
 
					
				
		
 lunminliang
		
			lunminliang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Question has been submitted as SR to technical support and ticket closed. Sharing below the comment of ticket for more community members reference:
You are using a strange data type code (0x22) in store commands. Please find below valid RNG job descriptors:
### rnggen_1
[00] B0800006 jobhdr: stidx=0 len=6
[01] 12820004 ld: ccb1-datasz len=4 offs=0 imm
[02] 00000020 data:0x00000020
[03] 82500000 operation: cls1-op rng (SH0) generate random
[04] 60300020 fifostr: msg len=32
[05] 00004020 ptr->@0x00004020
If the SEC4 is going to be doing other things, this will be a better examples:
### rnggen_2
[00] B8800303 shrhdr: stidx=0 share=always len=3
[01] 82500000 operation: cls1-op rng (SH0) generate random
[02] 68340020 seqfifostr: rng-ref len=32
OR
### rnggen_3
[00] B0800008 jobhdr: stidx=0 len=8
[01] 10FA0008 ld: ind-nfifo len=8 offs=0 imm
[02] 42F30000 <nfifo_entry: pad->class1 type=msg/rsvd0F
ptype=rnd
[03] 00000400 extlen=1024>
[04] 16860800 ld: deco-ctrl len=0 offs=8 imm -auto-nfifo-entries
[05] 7A920400 move: ififo->class1-alnblk -> ofifo, len=1024 (aux_ls)
[06] 60300400 fifostr: msg len=1024
[07] 00004400 ptr->@0x00004400
Note: #3 use the Info FIFO's "pad block" source for random data.
 
					
				
		
 lunminliang
		
			lunminliang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Question has been submitted as SR to technical support and ticket closed. Sharing below the comment of ticket for more community members reference:
You are using a strange data type code (0x22) in store commands. Please find below valid RNG job descriptors:
### rnggen_1
[00] B0800006 jobhdr: stidx=0 len=6
[01] 12820004 ld: ccb1-datasz len=4 offs=0 imm
[02] 00000020 data:0x00000020
[03] 82500000 operation: cls1-op rng (SH0) generate random
[04] 60300020 fifostr: msg len=32
[05] 00004020 ptr->@0x00004020
If the SEC4 is going to be doing other things, this will be a better examples:
### rnggen_2
[00] B8800303 shrhdr: stidx=0 share=always len=3
[01] 82500000 operation: cls1-op rng (SH0) generate random
[02] 68340020 seqfifostr: rng-ref len=32
OR
### rnggen_3
[00] B0800008 jobhdr: stidx=0 len=8
[01] 10FA0008 ld: ind-nfifo len=8 offs=0 imm
[02] 42F30000 <nfifo_entry: pad->class1 type=msg/rsvd0F
ptype=rnd
[03] 00000400 extlen=1024>
[04] 16860800 ld: deco-ctrl len=0 offs=8 imm -auto-nfifo-entries
[05] 7A920400 move: ififo->class1-alnblk -> ofifo, len=1024 (aux_ls)
[06] 60300400 fifostr: msg len=1024
[07] 00004400 ptr->@0x00004400
Note: #3 use the Info FIFO's "pad block" source for random data.
Hello,
I've just read your answer.
I tried to generate a simple random number @0x10000170 . But when I load the Job Descriptor Base Address into the Input Job Ring Register,
I haven't a Random number at the address @0x10000170...
### rnggen_1
[00] B0800006 jobhdr: stidx=0 len=6
[01] 12820004 ld: ccb1-datasz len=4 offs=0 imm
[02] 00000020 data:0x00000020
[03] 82500000 operation: cls1-op rng (SH0) generate random
[04] 60300020 fifostr: msg len=32
[05] 10000170 ptr->@0x10000170
... what is the problem with this descriptor ?
What I don't make well ?
Please, could you help me ?
Fabien.