P4080-PC Desktop Configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P4080-PC Desktop Configuration

Jump to solution
1,929 Views
rogergallion
Contributor II

Section 4.1 of the P4080DS-PC user's guide (https://www.freescale.com/files/32bit/doc/user_guide/P4080DSUG.pdf) shows the unit connected to a monitor/keyboard/mouse, but I find no connectors on the unit for connecting a monitor.  Am I missing something?

Labels (1)
0 Kudos
Reply
1 Solution
1,766 Views
rogergallion
Contributor II

Response from Fedor at Freescale Techniical Support:

Sorry, but this is a documentation issue - the P4080DS has only serial connector and has to be connected to a host-computer serial port.

I've reported the issue to the documentation group.

View solution in original post

0 Kudos
Reply
2 Replies
1,767 Views
rogergallion
Contributor II

Response from Fedor at Freescale Techniical Support:

Sorry, but this is a documentation issue - the P4080DS has only serial connector and has to be connected to a host-computer serial port.

I've reported the issue to the documentation group.

0 Kudos
Reply
1,766 Views
bpe
NXP Employee
NXP Employee

There is no video adapter on the main P4080DS board. Such adapter can be plugged

into one of the PCIe slots on P4080DS. Note, a video card is not included in

P4080DS shipment.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------