P4080-PC Desktop Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P4080-PC Desktop Configuration

ソリューションへジャンプ
1,930件の閲覧回数
rogergallion
Contributor II

Section 4.1 of the P4080DS-PC user's guide (https://www.freescale.com/files/32bit/doc/user_guide/P4080DSUG.pdf) shows the unit connected to a monitor/keyboard/mouse, but I find no connectors on the unit for connecting a monitor.  Am I missing something?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,767件の閲覧回数
rogergallion
Contributor II

Response from Fedor at Freescale Techniical Support:

Sorry, but this is a documentation issue - the P4080DS has only serial connector and has to be connected to a host-computer serial port.

I've reported the issue to the documentation group.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,768件の閲覧回数
rogergallion
Contributor II

Response from Fedor at Freescale Techniical Support:

Sorry, but this is a documentation issue - the P4080DS has only serial connector and has to be connected to a host-computer serial port.

I've reported the issue to the documentation group.

0 件の賞賛
返信
1,767件の閲覧回数
bpe
NXP Employee
NXP Employee

There is no video adapter on the main P4080DS board. Such adapter can be plugged

into one of the PCIe slots on P4080DS. Note, a video card is not included in

P4080DS shipment.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------