P3014 - Generic Machine Check Exception Handler

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P3014 - Generic Machine Check Exception Handler

1,844 Views
diwakarvasa
Contributor I

Hi Community, I'm using QorIQ P3041 board and I want to know how to write the generic machine check exception handler. Can someone help me?

I'm referring "EREF: A Programmer’s Reference Manual for Freescale Power Architecture Processors", Chapter 8, Section 8.7 Interrupt Processing.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,439 Views
Pavel
NXP Employee
NXP Employee

Look at attached files. Find the Machine Check interrupt handler in these files. These files contain interrupt handler procedures for the MPC85xx and QorIQ from CodeWarrior. Use this code as example for the P3041.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply