P3014 - Generic Machine Check Exception Handler

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P3014 - Generic Machine Check Exception Handler

1,870件の閲覧回数
diwakarvasa
Contributor I

Hi Community, I'm using QorIQ P3041 board and I want to know how to write the generic machine check exception handler. Can someone help me?

I'm referring "EREF: A Programmer’s Reference Manual for Freescale Power Architecture Processors", Chapter 8, Section 8.7 Interrupt Processing.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,465件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at attached files. Find the Machine Check interrupt handler in these files. These files contain interrupt handler procedures for the MPC85xx and QorIQ from CodeWarrior. Use this code as example for the P3041.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信