P2020 - SerDes equalization operation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P2020 - SerDes equalization operation

Jump to solution
1,711 Views
jeffbateman
Contributor I

In the P2020 QorIQ Integrated Processor Reference Manual, Rev. 2, 12/2012, paragraphs for registers GUTS_SRDSCR0 and GUTS_SRDSCR1 list SerDes Tx equalization settings. But, I'm having a hard time finding info about how the equalization operates. This is for a PCIe application, with a requirement to compensate for channel loss.

* Is it pre-emphasis, where the initial amplitude is increased above the final level set in SRDSCR5[SDTXL0..1] and SRDSCR6[SDTXL2..3]?

* Or is it de-emphasis, where the final amplitude is decreased below the initial level set in SRDSCR5[SDTXL0..1] and SRDSCR6[SDTXL2..3]?

* Or, something else?

* And, for how long does the pre / de-emphasis occur?

The only mention of emphasis or equalization I could find is in the P2020 QorIQ Integrated Processor Hardware Specifications, Rev. 2 manual, Para. 2.20.2 Equalization. But that's in the sRIO section, and is just a general discussion with no specifics relating to QorIQ devices.

Also:

* Is there an option to apply receiver equalization?

* Register GUTS_SRDSCR4 controls idle detection for lanes 2 & 3. Is there also a register for lanes 0 & 1?

  (curiously, there is no mention of GUTS_SRDSCR3 in the manual, which may or may not be for those lanes)

Thanks for your help.

P2020 QorIQ Integrated Processor Reference Manual, Rev. 2, 12/2012

Labels (1)
0 Kudos
Reply
1 Solution
1,459 Views
LPP
NXP Employee
NXP Employee

TXEQn defines de-emphasis.

De-emphasis attenuates the voltage level at the transmitter of all consecutive bits of the same signal state except the first. Full amplitude (defived by SDTXLn) is driven at the transmitter for one bit period of the transition bit.

Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,460 Views
LPP
NXP Employee
NXP Employee

TXEQn defines de-emphasis.

De-emphasis attenuates the voltage level at the transmitter of all consecutive bits of the same signal state except the first. Full amplitude (defived by SDTXLn) is driven at the transmitter for one bit period of the transition bit.

Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply