P1020RDB-PD board boot sequence configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P1020RDB-PD board boot sequence configuration

2,110件の閲覧回数
tomaszlenartowi
Contributor I

Hi,

I have a question regarding P1020RDB-PD board - will replacing the board's P1020 CPU micro with clean(out of the box) chip affect the boot sequence of the device? How is the board configured to start executing U Boot from NOR flash? Is it a hardware configuration?

Thanks.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,865件の閲覧回数
ufedor
NXP Employee
NXP Employee

> replacing the board's P1020 CPU micro with clean(out of the box) chip

What exactly do you mean, considering that the processor on the RDB board is soldered?

> How is the board configured to start executing U Boot from NOR flash?

By means of the on-board configuration switches.

0 件の賞賛
返信

1,865件の閲覧回数
tomaszlenartowi
Contributor I

I know, I meant actually re-soldering micro on the board.

So, if the configuration switches SW3 are not changed, re-soldering CPU will not affect the boot sequence, correct?

0 件の賞賛
返信

1,865件の閲覧回数
ufedor
NXP Employee
NXP Employee

Correct, if the processor of the same or higher speed grade is installed.

0 件の賞賛
返信