LTIB installation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LTIB installation

1,768件の閲覧回数
ashwingandhi
Contributor II

Hi,

am trying to install LTIB (ltib-13-2-1-sv) on Ubuntu 14.04 LTS. but getting error permission denied.

i want build image for P1013 processor(e500) core.

my question is "ltib-13-2-1-sv" is right version for e500 core and Ubuntu 14.04? if not please suggest me the correct version.

thanks

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,597件の閲覧回数
ashwingandhi
Contributor II

hi,

thanks for replay.

as you said i downloaded QorIQ SDK V1.9 PPCE500V2 IMAGE.iso before but i couldn't find document how install and use it.

can u please tel me how to use this SDK installation and configure files for the specific board.

thanks,

Ashwinkumar

0 件の賞賛
返信

1,597件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

LTIB is quite old system, not used now. Please use more recent yocto-based "Linux SDK for QorIQ Processors":

Linux® SDK for QorIQ Processors|NXP


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信