P1011 maximum clock input

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P1011 maximum clock input

1,975件の閲覧回数
danielminors
Contributor I

I cannot find any detail on the datasheet regarding the tolerance of the 100MHz maximum clock input for the P1011 processor. What is the maximum clock PPM that can be used when supplied with a 100MHz source?

0 件の賞賛
返信
2 返答(返信)

1,919件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

The 100MHz SYSCLK supports spread spectrum on P1011
So essentially there is no ppm restriction on this clock.

0 件の賞賛
返信

1,948件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Confirming with the AE team.

0 件の賞賛
返信