Not able to execute u-boot.bin flashing via Target Tasks in codewarrior IDE for P1022

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Not able to execute u-boot.bin flashing via Target Tasks in codewarrior IDE for P1022

ソリューションへジャンプ
3,429件の閲覧回数
aswinas017
Contributor I

I found the cheat sheet for burning u-boot through target tasks.

This is as follows.

Import XML--> I did for P1022DS_NOR_FLASH.xml.

Then add action-program/verify.

Added my u-boot.bin file and selected the options which are mentioned in the cheat sheet.

Finally when I try to execute it , the execute button is disabled.

How can I resolve this issue?

If anybody experienced with p1022 and NOR flash, please share the details which you follow.

Or anybody tried u-boot.bin successfully please share the steps.

Thanks dudes.

0 件の賞賛
返信
1 解決策
3,279件の閲覧回数
Pavel
NXP Employee
NXP Employee

The simplest way is the following:

Create a CodeWarrior Bareboard Project. See the ClipBoard04.jpg file.

Set "Run Configuration" to this project.

See attached Clipboard02.jpg.file.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
3,280件の閲覧回数
Pavel
NXP Employee
NXP Employee

The simplest way is the following:

Create a CodeWarrior Bareboard Project. See the ClipBoard04.jpg file.

Set "Run Configuration" to this project.

See attached Clipboard02.jpg.file.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------