Linux SDK 1.4 Installation Query

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux SDK 1.4 Installation Query

ソリューションへジャンプ
2,333件の閲覧回数
nishad_kamdar
Contributor IV

Hey community, thanks for considering this problem

I am trying to install SDK 1.4 on Ubuntu 12.10 for P1022DS machine.

I downloaded the Source and Cache and installed both of them as recommended.

I completed all the steps given until the step below which says:

For Ubuntu and Debian hosts (reconfigure /bin/sh to point to bash):

I am new to Linux and am following the steps blindly and would like to know what the sentence in the Curved Braces means and how i achieve it so that i could follow the further steps?

It would be helpful if someone could shed light on it.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,220件の閲覧回数
XXiao1z
Contributor III
sudo dpkg-reconfigure dash

then choose "No" and you're done.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,221件の閲覧回数
XXiao1z
Contributor III
sudo dpkg-reconfigure dash

then choose "No" and you're done.

0 件の賞賛
返信
2,220件の閲覧回数
nishad_kamdar
Contributor IV

I executed the above script and it seemed to work fine..

I have now started building the image..

Thanks,,

0 件の賞賛
返信