Linux SDK 1.4 Installation Query

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux SDK 1.4 Installation Query

Jump to solution
2,344 Views
nishad_kamdar
Contributor IV

Hey community, thanks for considering this problem

I am trying to install SDK 1.4 on Ubuntu 12.10 for P1022DS machine.

I downloaded the Source and Cache and installed both of them as recommended.

I completed all the steps given until the step below which says:

For Ubuntu and Debian hosts (reconfigure /bin/sh to point to bash):

I am new to Linux and am following the steps blindly and would like to know what the sentence in the Curved Braces means and how i achieve it so that i could follow the further steps?

It would be helpful if someone could shed light on it.

Labels (1)
0 Kudos
Reply
1 Solution
2,231 Views
XXiao1z
Contributor III
sudo dpkg-reconfigure dash

then choose "No" and you're done.

View solution in original post

0 Kudos
Reply
2 Replies
2,232 Views
XXiao1z
Contributor III
sudo dpkg-reconfigure dash

then choose "No" and you're done.

0 Kudos
Reply
2,231 Views
nishad_kamdar
Contributor IV

I executed the above script and it seemed to work fine..

I have now started building the image..

Thanks,,

0 Kudos
Reply