Linux SDK 1.4 Installation Query

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Linux SDK 1.4 Installation Query

跳至解决方案
1,453 次查看
nishad_kamdar
Contributor IV

Hey community, thanks for considering this problem

I am trying to install SDK 1.4 on Ubuntu 12.10 for P1022DS machine.

I downloaded the Source and Cache and installed both of them as recommended.

I completed all the steps given until the step below which says:

For Ubuntu and Debian hosts (reconfigure /bin/sh to point to bash):

I am new to Linux and am following the steps blindly and would like to know what the sentence in the Curved Braces means and how i achieve it so that i could follow the further steps?

It would be helpful if someone could shed light on it.

标签 (1)
0 项奖励
回复
1 解答
1,340 次查看
XXiao1z
Contributor III
sudo dpkg-reconfigure dash

then choose "No" and you're done.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,341 次查看
XXiao1z
Contributor III
sudo dpkg-reconfigure dash

then choose "No" and you're done.

0 项奖励
回复
1,340 次查看
nishad_kamdar
Contributor IV

I executed the above script and it seemed to work fine..

I have now started building the image..

Thanks,,

0 项奖励
回复