Is there a reference schematics available for P4080 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a reference schematics available for P4080 ?

1,200 Views
lokeshs
Contributor I

Planning to design a 6U VPX Board based on P4080 Processor.

A reference schematics on the P4080 will be helpful.

Labels (1)
0 Kudos
Reply
1 Reply

984 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

Available P4080 boards you can see on the NXP site

http://www.nxp.com/products/microcontrollers-and-processors/power-architecture-processors/qoriq-powe...

Excepting COM Express Carrier Board Schematics of P4080COME-DS-PB QorIQ Development System there is not public schematics for any P4080 reference designs on the NXP site. You also can ask the nearest NXP representative or create request for schematics (please see how Enter a Service Request to discuss confidential information )

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply