Help! p1010 not started!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help! p1010 not started!

2,056 Views
sergeymo
Contributor I

Hello, friends!

I can not run my card with a processor p1010. I can not create u-Boot SD-card to start. I download from nxp.com files: SDK1.9 for QorIQ (Image/Cache/Enviroument fille for SDK1.9). In env. i find directory Target_Board\p1010rdb adn not found u-boot bin-image for SDcard. I have found this file in subdir \p1020rdb, but it does not PBL block. This file is bad? Moreover, in a given environment are no commands BITBACKE,,,  although it refers readmy-file in this subdir.

Any sequence of commands I need to perform to create the right image in-boot SD-card in Envronment SDK1.9  (Virtual Host Enviroment: QorIQ DPAA SDK v1.9 PPCE500V2 with Virtual Host Enviroment)?

Если все так сложно, может кто вышлет бинарник для SD-card c u-boot-звгрузчиком? Просто плата новая, а спец по linux шибко занят. Конфигурация платы - p1010+DDR3+NAND+SPI_Flash+SD -копия p1010rdb-pb, без NOR/PLD. Или файл для платы p1010rdb-pb. Буду всемерно признателен!

Labels (1)
0 Kudos
Reply
1 Reply

1,923 Views
ufedor
NXP Employee
NXP Employee

Please try the following steps:

1) refer to the QorIQ SDK 1.9 Documentation, 3.2.1 Customizing U-Boot

2) the required file is conf/machine/p1010rdb.conf

3) modify UBOOT_MACHINES by adding P1010RDB-PB_36BIT_SDCARD_defconfig and/or P1010RDB-PB_SDCARD_defconfig

4) rebuild referring 1)

0 Kudos
Reply