Flash u-boot on p2020rdb

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash u-boot on p2020rdb

ソリューションへジャンプ
3,079件の閲覧回数
matt_tsai
Contributor I

Hi,

I would like to flash a u-boot image on the p2020rdb board. Assuming the original u-boot image is corrupted and the board cannot boot up, how I can flash the u-boot onto it? Also, is there a working u-boot image so that I can verify the method?

I do have an old CodeWarrior JTAG debugger but not sure where I can get the working software associated with it.

Thank you for your help.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,900件の閲覧回数
Pavel
NXP Employee
NXP Employee

NXP offers SDK 1.9 for the P2020RDB board. This SDK supports booting from SD card.

Write u-boot to SD card and use this card for booting if u-boot is damaged.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,900件の閲覧回数
matt_tsai
Contributor I

Hi Pavel,

Can you advise how to configure p2020rdb to use the u-boot code from different storage such as NOR flash, NAND flash, and SD card? Thank you!

0 件の賞賛
返信
2,900件の閲覧回数
matt_tsai
Contributor I

I found a legacy user manual that explains this. So the problem is solved. Thank you.

0 件の賞賛
返信
2,901件の閲覧回数
Pavel
NXP Employee
NXP Employee

NXP offers SDK 1.9 for the P2020RDB board. This SDK supports booting from SD card.

Write u-boot to SD card and use this card for booting if u-boot is damaged.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信