ECC Support on P2020rdb

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ECC Support on P2020rdb

1,224件の閲覧回数
aratarorome
Contributor I

Hello,

I use the P2020rdb from Freescale with VxWorks 6.9 and a compatible current BSP from WindRiver. When I want to activted the ECC support the boot loader did not boot anymore.

My question: Is the P2020rdb ready to use the ECC feature or not?

I ask because I found this comment in the VxWorks BSP:

/* possibly this is not supported check your DDR undefined for safety */

#undef  INCLUDE_DDR_ECC

I have the P2020RDB-PCA  Rev B.

Thanks in advance,

Andreas

ラベル(1)
0 件の賞賛
返信
1 返信

1,018件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

The P2020RDB-PCA rev.B is not ready to use the ECC feature. It has 64-bit DDR memory (4 x 16-bit DDR devices). There is not DDR memory device for ECC on the P2020rdb nor place to install it.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信