Dynamically resolve ARP upon ipfwd application

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Dynamically resolve ARP upon ipfwd application

1,608件の閲覧回数
shanfeifei
Fresh Out Contributor

The SDK1.6 says that:Note that ipfwd application does not dynamically resolve ARP – missing ARP entries will result in the application dropping the packet.

So how to dynamically resolve ARP? Modify the code of ipfwd application?

ラベル(1)
タグ(4)
0 件の賞賛
返信
2 返答(返信)

1,476件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello shan feifei,

USDPAA IPFWD could response ARP request, but won't send ARP request to resolve ARP, thus ARP entries needs to be hard coded in configuration script.

Yes, you need additional development, to support dynamic ARP:

1. Implement in IPFWD application.

2. Offload to Linux, get it from there and cache to IPFWD application.

Is it urgent?


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,476件の閲覧回数
shanfeifei
Fresh Out Contributor

Hi,Lunmin,thank you for your reply!

It is a little urgent,so do you have some ready-made C codes for resolving ARP?

0 件の賞賛
返信