Custom P2041 board DDR problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Custom P2041 board DDR problem

1,914 次查看
ayhmi
Contributor II

Hello,

We are using a custom P2041 board. We were working with u-boot without a problem for 2 months. Last week with no reason u-boot hangs on DDR initialization. After i debugged i realized that DDR controller initialization passes (D_INIT bit is cleared) but read/write procedures to RAM fails. I mean i can't read the same data i wrote.

I checked my board and observed that P2041 sends constantly DDR reset to RAM modules. I can think source of the problem may be following:

- SDRAM hardware problem

- P2041 hardware problem

- DDR controller initialization problem (It was working before)

We are using 5xISSI IS43TR16512A-15HBLI 512Mx16 8Gb DDR3 SDRAM with ECC. If anyone experienced similar problem please help me to determine the source of problem.

Thanks

标签 (1)
标记 (3)
0 项奖励
回复
2 回复数

1,656 次查看
Bulat
NXP Employee
NXP Employee

As far as I know P2041 does not have dedicated "DDR reset" signal. When you observed that P2041 sends constantly DDR reset to RAM modules, which P2041 signal you checked? Or more general, how DDR reset is generated on your board?

Regards,

Bulat

0 项奖励
回复

1,656 次查看
ayhmi
Contributor II

I am sorry i misjudged the situation. Yes you are right Bulat. Hardware signals seem correct. However RAM data changes between 2 memory reads.

0 项奖励
回复