Codewarrior Connect Failure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior Connect Failure

ソリューションへジャンプ
3,407件の閲覧回数
sivakrishnaravi
Contributor I

Our Objective to erase the flash on the P2020AMC

With the help of expansion card i am trying to connect using JTAG (Codewarrior USB TAP COP)

I have installed the CodeWarrior for Power Architecture v10.2.1 and trying to use the Flash Programmer.

But while trying to establish connection i am getting the connect failed error.

The screenshot is attached. If any one have encountered similar error please respond.

Thanks,

Siva Krishna R

ラベル(1)
0 件の賞賛
返信
1 解決策
2,825件の閲覧回数
lunminliang
NXP Employee
NXP Employee

I guess this is related to the "Target Initialization file", please make sure you are using the corrected target initialization file, which You can find some information about in document Targeting PA Processors.pdf in C:\Program Files\Freescale\CW PA v10.x\PA\Help\PDF.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,826件の閲覧回数
lunminliang
NXP Employee
NXP Employee

I guess this is related to the "Target Initialization file", please make sure you are using the corrected target initialization file, which You can find some information about in document Targeting PA Processors.pdf in C:\Program Files\Freescale\CW PA v10.x\PA\Help\PDF.

0 件の賞賛
返信