Codewarrior Connect Failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior Connect Failure

Jump to solution
3,425 Views
sivakrishnaravi
Contributor I

Our Objective to erase the flash on the P2020AMC

With the help of expansion card i am trying to connect using JTAG (Codewarrior USB TAP COP)

I have installed the CodeWarrior for Power Architecture v10.2.1 and trying to use the Flash Programmer.

But while trying to establish connection i am getting the connect failed error.

The screenshot is attached. If any one have encountered similar error please respond.

Thanks,

Siva Krishna R

Labels (1)
0 Kudos
Reply
1 Solution
2,843 Views
lunminliang
NXP Employee
NXP Employee

I guess this is related to the "Target Initialization file", please make sure you are using the corrected target initialization file, which You can find some information about in document Targeting PA Processors.pdf in C:\Program Files\Freescale\CW PA v10.x\PA\Help\PDF.

View solution in original post

0 Kudos
Reply
1 Reply
2,844 Views
lunminliang
NXP Employee
NXP Employee

I guess this is related to the "Target Initialization file", please make sure you are using the corrected target initialization file, which You can find some information about in document Targeting PA Processors.pdf in C:\Program Files\Freescale\CW PA v10.x\PA\Help\PDF.

0 Kudos
Reply