Can't program P1010RDB Nand Flash with Codewarrior 10.3.3 & Codewarrior TAP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't program P1010RDB Nand Flash with Codewarrior 10.3.3 & Codewarrior TAP

Jump to solution
4,175 Views
franka
Contributor III

Hi,


I am looking for a few hints on why I can't re-program a P1010RDB development system NAND flash with CW 10.3.3 and CW USB TAP.  I was programming new u-boot images via u-boot through the serial console and that worked fine.  I then proceeded to flash an image that causes u-boot to lock-up as it boots.  Now I need to re-program the NAND flash with a working u-boot image.


I keep getting -

Did not erase bad block at address 0x00000000   Error:  Erase failed.


I am using all the default software packages as supplied with CW 10.3.3 with no modifications.  It appears to read the device ID.  I've enabled as much logging as I can find in CW.  Not sure what the issue is.  Below is the last log.  I was just trying to program the small bootloader in u-boot so that only one sector had to be erased.  The larger u-boot images do the exact same thing.  Thanks for any ideas.


fl::target -lc "FlashProgramElf0_Debug_P1010_Download"

fl::target -b 0x2000 0x30000

fl::target -v off -l on

cmdwin::fl::device -d "K9F5608Ux0D-IFC" -o "32Mx8x1" -a 0x0 0x1ffffff

cmdwin::fl::image -f "C:\\Users\\Frank\\Documents\\u-boot-git-r17\\git\\P1010RDB_NAND\\nand_spl\\u-boot-spl.bin" -t "Auto Detect" -re on -r 0x0 0x1ffffff -oe on -o 0x0

cmdwin::fl::erase image

Beginning Operation ...   

-------------------------

    log: Trying auto-detect...

    log:   File is NOT of type Motorola S-Record Format.

    log:   File is NOT of type Elf Format.

Auto-detection is successful.  

  File is of type Binary/Raw Format.  

    log: Using Algorithm: K9F5608x0D-IFC.elf

    log: 

    log: 

    log: ======================================================================

    log: === Target Configuration Settings

    log: === Launch Configuration:       FlashProgramElf0_Debug_P1010_Download

    log: ======================================================================

    log: Connecting ...

Performing target initialization ...   

    log: Connected ...

    log: 

    log: ======================================================================

    log: === Execute:              Erase

    log: === Timestamp:            Fri Jul 11 17:25:31 2014

    log: === Flash Device:         K9F5608Ux0D-IFC

    log: === Flash Organization:   32Mx8x1

    log: === Flash Mem Start Addr: 0x00000000

    log: === Flash Mem End Addr:   0x01FFFFFF

    log: ======================================================================

Downloading Flash Device Driver ...  

    log: Loading Flash Device Driver at: 0x00002000

    log: Flash Driver Buffer is at:  0x00006260

    log: Flash Driver Buffer Size is:  0x0002BDA0

    log: 

    log: Writing the Address 

    log: Writing the address of the sector list 

    log: Clearing the status 

    log: Setting up Registers 

    log: Commanding target to run 

Reading flash ID ...

    log: Reading init return status 

    log: Done

    log: 

    log: Initialization Command Succeeded

    log: Writing Erase Function Code 

    log: Writing the Address 

    log: Writing the Number of Sectors 

    log: Writing the address of the sector list 

    log: Writing the sector list 

Erasing Sector 0x00000000 to 0x00003FFF  

    log: Clearing the status 

    log: Setting up Registers 

    log: Commanding target to run 

Erasing ...

    log: Reading erase return status 

Did not erase bad block at address 0x00000000  

Error:  Erase failed.

    log: Timestamp:  Fri Jul 11 17:25:36 2014

Error: Erase failed.

 

Frank

Labels (1)
0 Kudos
Reply
1 Solution
3,464 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Frank,


The default initialization file in CodeWarrior 10.3.3 is for P1010RDB-PB with NAND Flash MT29F16G08ABABAWP, but it seems that you are using P1010RDB-PA, the IFC configuration in the default initialization file is not suitable for your target.

Please use the attached initialization file for P1010RDB-PA.

Have a great day,

Yiping Wang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
6 Replies
3,465 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Frank,


The default initialization file in CodeWarrior 10.3.3 is for P1010RDB-PB with NAND Flash MT29F16G08ABABAWP, but it seems that you are using P1010RDB-PA, the IFC configuration in the default initialization file is not suitable for your target.

Please use the attached initialization file for P1010RDB-PA.

Have a great day,

Yiping Wang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,464 Views
franka
Contributor III

Hi Yiping,

  Thank you for your reply.  I don't have access to my computer until next week.  I will use this init file next week and let you know what I find.

Frank

0 Kudos
Reply
3,464 Views
franka
Contributor III

Hi Yiping,

Still can't re-program the flash.  It says it's programmed now but the board does not boot.  Below are the three logs: 1) init debug CW, 2) flash programming and 3) nand boot.  I verified that all the switches on the P1010RDB board are configured exactly as the quick start guide advises.  I'm not sure why it says "NAND boot...skipping?"  Any ideas what's wrong?  Thanks.

1) CW init

Executing Initialization File: C:\Freescale\CW_PA_v10.3.3\PA\PA_Support\Initialization_Files\QorIQ_P1\P1010RDB_init_sram_flash.tcl
radix x
cmdwin::eclipse::config hexprefix 0x
cmdwin::eclipse::config MemIdentifier v
cmdwin::eclipse::config MemWidth 32
cmdwin::eclipse::config MemAccess 32
cmdwin::eclipse::config MemSwap off
cmdwin::mem p:0xff7e0004 -np
thread break: Stopped, 0x0, 0x0, cpuPowerPCBig, nand_ifc_flash_alg_debug.elf (state, tid, pid, cpu, target)
cmdwin::mem p:0xff700000 = 0x000e0000
cmdwin::mem p:0xe001e010 = 0x00000100
cmdwin::mem p:0xe0020e44 = 0x0000000C
cmdwin::reg Standard Special Purpose Registers/MSR = 0x02000200
cmdwin::reg regPPCTLB1/L2MMU_CAM0 = 0x70000FCAFC080000FF000000FF000001
cmdwin::reg regPPCTLB1/L2MMU_CAM1 = 0x70000FCAFC080000FE000000FE000001
cmdwin::reg regPPCTLB1/L2MMU_CAM2 = 0x500003CAFC080000E0000000E0000001
cmdwin::reg regPPCTLB1/L2MMU_CAM3 = 0x400001C0FC0800000000000000000001
cmdwin::reg regPPCTLB1/L2MMU_CAM4 = 0x400001CA1C080000EFB00000EFB00001
cmdwin::reg regPPCTLB1/L2MMU_CAM5 = 0x2000004A1C080000EFA00000EFA00001
cmdwin::mem p:0xe0000020 = 0x00000000
cmdwin::mem p:0xe001e010 = 0x00000100
cmdwin::mem p:0xe0020000 = 0x50010000
cmdwin::mem p:0xe0020100 = 0x00000000
cmdwin::mem p:0xe0020104 = 0x00000000
cmdwin::mem p:0xe0020000 = 0x90010000
cmdwin::mem p:0xe0000c08 = 0x000fe000
cmdwin::mem p:0xe0000c10 = 0x80400018
cmdwin::mem p:0xe0000c28 = 0x000efb00
cmdwin::mem p:0xe0000c30 = 0x80400010
cmdwin::mem p:0xe0000c48 = 0x00efa00
cmdwin::mem p:0xe0000c50 = 0x8040000d
cmdwin::mem p:0xe00e0060 = 0x000000c0
cmdwin::mem p:0xe001e0a0 = 0xFFFF0000
cmdwin::mem p:0xe001e130 = 0x00800000
cmdwin::mem p:0xe001e1c0 = 0x020C0405
cmdwin::mem p:0xe001e1c4 = 0x1D1D070C
cmdwin::mem p:0xe001e1c8 = 0x0180280F
cmdwin::mem p:0xe001e1cc = 0x04000000
cmdwin::mem p:0xe001e010 = 0xEFA00083
cmdwin::mem p:0xe001e0ac = 0xFE000000
cmdwin::mem p:0xe001e13c = 0x0000E000
cmdwin::mem p:0xe001e1f0 = 0x40050005
cmdwin::mem p:0xe001e1f4 = 0x1e000f00
cmdwin::mem p:0xe001e1f8 = 0x0410001c
cmdwin::mem p:0xe001e1fc = 0x00000000
cmdwin::mem p:0xe001e01c = 0xFE000101
cmdwin::mem p:0xe001e034 = 0xEFB00085
cmdwin::mem p:0xe001e0c4 = 0xFFFF0000
cmdwin::mem p:0xe001e154 = 0x00000000
cmdwin::mem p:0xe001e250 = 0xe00e000e
cmdwin::mem p:0xe001e254 = 0x0e001f00
cmdwin::mem p:0xe001e258 = 0x0e00001f
cmdwin::mem p:0xe001e25c = 0x00000000
cmdwin::mem p:0xe001e40c = 0x0e008000
cmdwin::mem p:0xe001e44c = 0x00000800
cmdwin::mem p:0xe0007000 = 0x80000403
cmdwin::mem p:0xe0007008 = 0x0000FB00
cmdwin::mem p:0xe0007020 = 0x28170008
cmdwin::reg e500 Special Purpose Registers/IVPR = 0x00000000
cmdwin::reg e500 Special Purpose Registers/IVOR0 = 0x00000100
cmdwin::reg e500 Special Purpose Registers/IVOR1 = 0x00000200
cmdwin::reg e500 Special Purpose Registers/IVOR2 = 0x00000300
cmdwin::reg e500 Special Purpose Registers/IVOR3 = 0x00000400
cmdwin::reg e500 Special Purpose Registers/IVOR4 = 0x00000500
cmdwin::reg e500 Special Purpose Registers/IVOR5 = 0x00000600
cmdwin::reg e500 Special Purpose Registers/IVOR6 = 0x00000700
cmdwin::reg e500 Special Purpose Registers/IVOR8 = 0x00000c00
cmdwin::reg e500 Special Purpose Registers/IVOR10 = 0x00000900
cmdwin::reg e500 Special Purpose Registers/IVOR11 = 0x00000f00
cmdwin::reg e500 Special Purpose Registers/IVOR12 = 0x00000b00
cmdwin::reg e500 Special Purpose Registers/IVOR13 = 0x00001100
cmdwin::reg e500 Special Purpose Registers/IVOR14 = 0x00001000
cmdwin::reg e500 Special Purpose Registers/IVOR15 = 0x00001500
cmdwin::reg e500 Special Purpose Registers/IVOR32 = 0x00001600
cmdwin::reg e500 Special Purpose Registers/IVOR33 = 0x00001700
cmdwin::reg e500 Special Purpose Registers/IVOR34 = 0x00001800
cmdwin::reg e500 Special Purpose Registers/IVOR35 = 0x00001900
cmdwin::mem v:0x00000700 = 0x48000000
cmdwin::mem v:0x00001500 = 0x48000000
cmdwin::reg e500 Special Purpose Registers/IAC1 = 0xfffffffc
cmdwin::reg e500 Special Purpose Registers/DBCR0 = 0x40800000
cmdwin::reg e500 Special Purpose Registers/DBCR1 = 0x00000000
cmdwin::eclipse::config runcontrolsync off
cmdwin::go
cmdwin::wait 50
cmdwin::eclipse::config runcontrolsync on
cmdwin::stop
thread break: Stopped, 0x0, 0x0, cpuPowerPCBig, nand_ifc_flash_alg_debug.elf (state, tid, pid, cpu, target)
cmdwin::reg e500 Special Purpose Registers/DBSR = 0x01CF0000
cmdwin::reg e500 Special Purpose Registers/DBCR0 = 0x41000000
cmdwin::reg e500 Special Purpose Registers/IAC1 = 0x00000000
cmdwin::reg e500 Special Purpose Registers/CSRR0 = 0x00000000
cmdwin::reg e500 Special Purpose Registers/CSRR1 = 0x00000000
cmdwin::reg Standard Special Purpose Registers/MSR = 0x02001200
cmdwin::reg e500 Special Purpose Registers/HID0 = 0x00004080
cmdwin::reg e500 Special Purpose Registers/DBCR0 = 0x41000000
cmdwin::reg General Purpose Registers/SP = 0x0000000F

2) Programming

fl::target -lc "NAND_IFC_Example-core00_RAM_P1010_Download"

fl::target -b 0x8000 0x40000

fl::target -v on -l on

cmdwin::fl::device -d "K9F5608Ux0D-IFC" -o "32Mx8x1" -a 0x0 0x1ffffff

cmdwin::fl::image -f "C:\\Users\\Frank\\Documents\\Freescale CodeWarrior Tools\\u-boot_nand.bin" -t "Auto Detect" -re on -r 0x0 0x1ffffff -oe on -o 0x0

cmdwin::fl::erase image

Beginning Operation ...   

-------------------------

    log: Trying auto-detect...

    log:   File is NOT of type Motorola S-Record Format.

    log:   File is NOT of type Elf Format.

Auto-detection is successful.  

  File is of type Binary/Raw Format.  

    log: Using Algorithm: K9F5608x0D-IFC.elf

    log: 

    log: 

    log: ======================================================================

    log: === Target Configuration Settings

    log: === Launch Configuration:       NAND_IFC_Example-core00_RAM_P1010_Download

    log: ======================================================================

    log: Connecting ...

Performing target initialization ...   

    log: Connected ...

    log: 

    log: ======================================================================

    log: === Execute:              Erase

    log: === Timestamp:            Sun Jul 20 11:28:29 2014

    log: === Flash Device:         K9F5608Ux0D-IFC

    log: === Flash Organization:   32Mx8x1

    log: === Flash Mem Start Addr: 0x00000000

    log: === Flash Mem End Addr:   0x01FFFFFF

    log: ======================================================================

Downloading Flash Device Driver ...  

    log: Loading Flash Device Driver at: 0x00008000

    log: Flash Driver Buffer is at:  0x0000C260

    log: Flash Driver Buffer Size is:  0x0003BDA0

    log: 

    log: Writing the Address 

    log: Writing the address of the sector list 

    log: Clearing the status 

    log: Setting up Registers 

    log: Commanding target to run 

Reading flash ID ...

    log: Reading init return status 

    log: Done

    log: 

    log: Initialization Command Succeeded

    log: Writing Erase Function Code 

    log: Writing the Address 

    log: Writing the Number of Sectors 

    log: Writing the address of the sector list 

    log: Writing the sector list 

Erasing Sector 0x00000000 to 0x00003FFF  

Erasing Sector 0x00004000 to 0x00007FFF  

Erasing Sector 0x00008000 to 0x0000BFFF  

Erasing Sector 0x0000C000 to 0x0000FFFF  

Erasing Sector 0x00010000 to 0x00013FFF  

Erasing Sector 0x00014000 to 0x00017FFF  

Erasing Sector 0x00018000 to 0x0001BFFF  

Erasing Sector 0x0001C000 to 0x0001FFFF  

Erasing Sector 0x00020000 to 0x00023FFF  

Erasing Sector 0x00024000 to 0x00027FFF  

Erasing Sector 0x00028000 to 0x0002BFFF  

Erasing Sector 0x0002C000 to 0x0002FFFF  

Erasing Sector 0x00030000 to 0x00033FFF  

Erasing Sector 0x00034000 to 0x00037FFF  

Erasing Sector 0x00038000 to 0x0003BFFF  

Erasing Sector 0x0003C000 to 0x0003FFFF  

Erasing Sector 0x00040000 to 0x00043FFF  

Erasing Sector 0x00044000 to 0x00047FFF  

Erasing Sector 0x00048000 to 0x0004BFFF  

Erasing Sector 0x0004C000 to 0x0004FFFF  

Erasing Sector 0x00050000 to 0x00053FFF  

Erasing Sector 0x00054000 to 0x00057FFF  

Erasing Sector 0x00058000 to 0x0005BFFF  

Erasing Sector 0x0005C000 to 0x0005FFFF  

Erasing Sector 0x00060000 to 0x00063FFF  

    log: Clearing the status 

    log: Setting up Registers 

    log: Commanding target to run 

Erasing ...

    log: Reading erase return status 

    log: Done

Erase Command Succeeded   

    log: Timestamp:  Sun Jul 20 11:28:34 2014

cmdwin::fl::write verify

-------------------------

Using restricted address range 0x00000000 to 0x01FFFFFF  

Programming file C:\Users\Frank\Documents\Freescale CodeWarrior Tools\u-boot_nand.bin  

    log: Trying auto-detect...

    log:   File is NOT of type Motorola S-Record Format.

    log:   File is NOT of type Elf Format.

Auto-detection is successful.  

  File is of type Binary/Raw Format.  

    log: Using Algorithm: K9F5608x0D-IFC.elf

    log: 

    log: ======================================================================

    log: === Execute:              Program

    log: === Timestamp:            Sun Jul 20 11:28:34 2014

    log: === Flash Device:         K9F5608Ux0D-IFC

    log: === Flash Organization:   32Mx8x1

    log: === Flash Mem Start Addr: 0x00000000

    log: === Flash Mem End Addr:   0x01FFFFFF

    log: ======================================================================

Downloading Flash Device Driver ...  

    log: Loading Flash Device Driver at: 0x00008000

    log: Flash Driver Buffer is at:  0x0000C260

    log: Flash Driver Buffer Size is:  0x0003BDA0

    log: 

    log: Writing the Address 

    log: Writing the address of the sector list 

    log: Clearing the status 

    log: Setting up Registers 

    log: Commanding target to run 

Reading flash ID ...

    log: Reading init return status 

    log: Done

    log: 

    log: Initialization Command Succeeded

    log: Trying auto-detect...

    log:   File is NOT of type Motorola S-Record Format.

    log:   File is NOT of type Elf Format.

Auto-detection is successful.  

  File is of type Binary/Raw Format.  

Downloading 0x00010000 bytes to be programmed at 0x00000000  

Downloading 0x00010000 bytes to be programmed at 0x00010000  

Downloading 0x00010000 bytes to be programmed at 0x00020000  

    log: Programming 0x00010000 bytes of Target Memory at 0x00000000

    log: Writing Program Function Code 

    log: Writing the Address 

    log: Writing the Size 

    log: Writing the address of the buffer 

    log: Clearing the status 

    log: Setting up Registers 

    log: Commanding target to run 

Executing program with verify ....  

    log: Reading program return status 

Program with Verify Command Succeeded   

Downloading 0x00010000 bytes to be programmed at 0x00030000  

Downloading 0x00010000 bytes to be programmed at 0x00040000  

Downloading 0x00010000 bytes to be programmed at 0x00050000  

Downloading 0x00000C88 bytes to be programmed at 0x00060000  

    log: Programming 0x00000C88 bytes of Target Memory at 0x00030000

    log: Writing Program Function Code 

    log: Writing the Address 

    log: Writing the Size 

    log: Writing the address of the buffer 

    log: Clearing the status 

    log: Setting up Registers 

    log: Commanding target to run 

Executing program with verify ....  

    log: Reading program return status 

Program with Verify Command Succeeded   

    log: Programmed total of 0x00060C88 bytes

    log: 

    log: Timestamp:  Sun Jul 20 11:28:41 2014

3) Board boot

NAND boot... skipping


U-Boot 2010.12-00063-g8669298-dirty (Jul 09 2011 - 12:42:30)

CPU:   P1010E, Version: 1.0, (0x80f90010)
Core:  E500, Version: 5.1, (0x80212151)
Clock Configuration:
       CPU0:800  MHz,
       CCB:400  MHz,
       DDR:333.333 MHz (666.667 MT/s data rate) (Asynchronous), IFC:100  MHz
L1:    D-cache 32 kB enabled
       I-cache 32 kB enabled
Board: P1010RDB
I2C:   ready
SPI:   ready
DRAM:  Detected UDIMM(s)
1 GiB (DDR3, 32-bit, CL=5, ECC off)
FLASH: *** failed ***
### ERROR ### Please RESET the board ###

- every time I reset I get the exact same boot messages.

Frank

0 Kudos
Reply
3,464 Views
franka
Contributor III

Hi Yiping,

I was verifying the jumper settings on the P1010RDB and I noticed that I must have changed J34 from the default position as listed on the schematic.  I changed J34 back to position 2-3 (Default) and it appears I can boot from NAND flash now.  I have more testing to completely verify but it looks promising.  Not sure why J34 would have any effect on a NAND boot when schematically it appears as only connected to the NOR flash?

Frank

0 Kudos
Reply
3,465 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Frank,

There is no error in the flash programmer log. In the u-boot log, it just fails at NOR Flash detecting, you could compare the error log with the successful boot log, so J34 connect configuration is needed.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,464 Views
franka
Contributor III

Hi Yiping,

The P1010RDB boots successfully now.

Frank

0 Kudos
Reply