SPI Interface of P1010

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI Interface of P1010

1,088 Views
weizhansong
Contributor I

Hello,

  We want to use P1010 at slave state when we using the SPI interface, but now we can no find a bit the set master or slave.

So we want to ask that is it OK to use P1010 as salve mode? If ok ,how can we set the status?Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

913 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Weizhan,

P1010 eSPI controller doesn't support slave mode, so I think it is impossible to configure P1010 at slave mode, please refer to "Chapter 18 Enhanced Serial Peripheral Interface" in P1010RM. Probably you could choose PCIe EP mode.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply