CECR[RST] bit won't clear.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CECR[RST] bit won't clear.

1,448 Views
eng5678
Contributor I

Is there any reason why the powequicc risc processor wont clear the CECR[FLAG] bit when a command is issued?  I have issued a command and am polling on this bit for completion but it never clears.  Only a CECR[RST] =1 clears it.

Labels (1)
0 Kudos
Reply
2 Replies

1,316 Views
eng5678
Contributor I

The root problem for this question was corrected by loading microcode into the quicc engine.  Our experience has been primarily with Powerquicc 2 CPMs (MPC82XX) which have the microcode preloaded. 

0 Kudos
Reply

1,316 Views
LPP
NXP Employee
NXP Employee

1.

QE may halt if it's clocks frequencies are out of range. Please check QE PLL and VCO frequency (and also frequencies of serial interfaces) .

2.

QE may halt because of bus error (before init_tx_rx command or as the result of this command). Check SDMA Status register SDSR. If error is set, check SDTA1/SDTA2/SDTM1/SDTM2 registers.

3.

The QE never crashes!

- It can stop completely on SDMA faults. You should always have an error handler for this!

- It works with all data/parameters you give it. Wrong parameters may cause fault!

- MURAM Parameter overlaps cause mostly very interesting effects of highly statistical nature.

- Structure alignment messups are the 2nd most common problem.

Are you sure that QE has been running before a new command was issued? Have you try other QE protocols running (e.g. UART)?

4.

Hint. On bootup with disabled QE:

Set complete MURAM to some “odd” value (not zeroes!), e.g., 0x55 that can easily be identified in broken pointers or missing initializations.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply