Booting issue in P1022 based target :: core0 in wait mode and core1 in run mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Booting issue in P1022 based target :: core0 in wait mode and core1 in run mode

1,285 次查看
rammurmu
Contributor III

In normal scenarios for P1022 based target , core0 is kept in run mode and core1 in wait mode. In this case kernel boot is OK.

However when core0 is kept in wait mode and core1 in run mode, there is problem is kernel booting. The part of error log is -

smp_85xx_kick_cpu: timeout waiting for core 1 to ack
smp: failed starting cpu 0 (rc -2)
Brought up 1 CPUs
Do we have to change some configuration of kernel when core0 is set in wait mode and core1 is in run mode using POR configuration.
Regards
Ram
标签 (1)
0 项奖励
回复
1 回复

1,178 次查看
rammurmu
Contributor III

Found the solution -

Compile the dts with the following arguments -

./dtc -O dtb -o p1022ds_xgm.dtb -b 1 p1022ds_32b.dts

Where '1' specifies the boot cpu id.

Now it works

Regards

Ram

0 项奖励
回复