Auto CPO for DDR2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Auto CPO for DDR2

Jump to solution
1,834 Views
yansongzhu
Contributor III

During configuring the DDR controller of the P2020, I want to know whether the auto cpo setting(automatic CAS to preamble calibration) is effective for DDR2 ? And is it the recommended setting ?

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
1,684 Views
Bulat
NXP Employee
NXP Employee

Yes, auto CPO setting is effective for DDR2. This setting was used in SDK 1.7 for P2020RDB (with DDR2).

Regards,

Bulat

View solution in original post

2 Replies
1,685 Views
Bulat
NXP Employee
NXP Employee

Yes, auto CPO setting is effective for DDR2. This setting was used in SDK 1.7 for P2020RDB (with DDR2).

Regards,

Bulat

1,684 Views
yansongzhu
Contributor III

Thanks!

0 Kudos
Reply