Auto CPO for DDR2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,831件の閲覧回数
yansongzhu
Contributor III

During configuring the DDR controller of the P2020, I want to know whether the auto cpo setting(automatic CAS to preamble calibration) is effective for DDR2 ? And is it the recommended setting ?

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,681件の閲覧回数
Bulat
NXP Employee
NXP Employee

Yes, auto CPO setting is effective for DDR2. This setting was used in SDK 1.7 for P2020RDB (with DDR2).

Regards,

Bulat

元の投稿で解決策を見る

2 返答(返信)
1,682件の閲覧回数
Bulat
NXP Employee
NXP Employee

Yes, auto CPO setting is effective for DDR2. This setting was used in SDK 1.7 for P2020RDB (with DDR2).

Regards,

Bulat

1,681件の閲覧回数
yansongzhu
Contributor III

Thanks!

0 件の賞賛
返信