Assign memory address to DDR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Assign memory address to DDR

跳至解决方案
1,087 次查看
敏赵
Contributor I

Hi,

The size of my DDR chip is 4GB, can I only assign 1GB memory address to it?

Best regards,

Min Zhao

标签 (1)
0 项奖励
回复
1 解答
912 次查看
catalindemergia
Contributor IV

Yes, you have to specify:

the base address that you want from Local Access Window Base Address Register

the size (1 GB in your case) from the Local Access Window Attributes Register - it has the SIZE field in it, bits 26-31

regards,

Catalin

在原帖中查看解决方案

0 项奖励
回复
1 回复
913 次查看
catalindemergia
Contributor IV

Yes, you have to specify:

the base address that you want from Local Access Window Base Address Register

the size (1 GB in your case) from the Local Access Window Attributes Register - it has the SIZE field in it, bits 26-31

regards,

Catalin

0 项奖励
回复