-

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
2,403 Views
ymha07
Contributor II

Moved to P series forum

==========================================================================

Wireless 1588 communications with P2020RDB-PCA

Hi, 

I want to try to construct a Wireless LAN using P2020RDB-PCAs with QorIQ SDK 1.9.

However, it seems difficult to find available wireless modules and drivers that support the platform.

Could you please recommend modules and drivers?

Moreover, is it possible to use IEEE 1588 hardware time stamping for wireless communications? 

Or do I have to use software time stamping?

Thanks in advance for your help.

 

 

Tags (2)
0 Kudos
Reply
1 Solution
2,373 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following link.

https://community.nxp.com/t5/QorIQ/after-install-ath10k-pci-module-on-ls1021a-TWR-Eva-wlp1s0-scan/m-...

 

In addition, it is impossible to use IEEE 1588 hardware time stamping for wireless communications

 

View solution in original post

2 Replies
2,374 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following link.

https://community.nxp.com/t5/QorIQ/after-install-ath10k-pci-module-on-ls1021a-TWR-Eva-wlp1s0-scan/m-...

 

In addition, it is impossible to use IEEE 1588 hardware time stamping for wireless communications

 

2,343 Views
ymha07
Contributor II

Thank you for the reply.

I will refer to the link

0 Kudos
Reply