-

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,405件の閲覧回数
ymha07
Contributor II

Moved to P series forum

==========================================================================

Wireless 1588 communications with P2020RDB-PCA

Hi, 

I want to try to construct a Wireless LAN using P2020RDB-PCAs with QorIQ SDK 1.9.

However, it seems difficult to find available wireless modules and drivers that support the platform.

Could you please recommend modules and drivers?

Moreover, is it possible to use IEEE 1588 hardware time stamping for wireless communications? 

Or do I have to use software time stamping?

Thanks in advance for your help.

 

 

タグ(2)
0 件の賞賛
返信
1 解決策
2,375件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following link.

https://community.nxp.com/t5/QorIQ/after-install-ath10k-pci-module-on-ls1021a-TWR-Eva-wlp1s0-scan/m-...

 

In addition, it is impossible to use IEEE 1588 hardware time stamping for wireless communications

 

元の投稿で解決策を見る

2 返答(返信)
2,376件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following link.

https://community.nxp.com/t5/QorIQ/after-install-ath10k-pci-module-on-ls1021a-TWR-Eva-wlp1s0-scan/m-...

 

In addition, it is impossible to use IEEE 1588 hardware time stamping for wireless communications

 

2,345件の閲覧回数
ymha07
Contributor II

Thank you for the reply.

I will refer to the link

0 件の賞賛
返信