s32R294

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
6,442 Views
iceice
Contributor III

请问,s32r294两个射频前端怎么切换的,1个SPT模块怎么处理两个射频数据呢

0 Kudos
Reply
1 Solution
6,271 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Yes, this is possible.

The S32R294 supports connection of 2 front end AFEs.

Best regards,

Peter

View solution in original post

0 Kudos
Reply
11 Replies
6,435 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Unfortunately this is English forum. Could you place your question in English as google translate of your question is quite blurry.

Best regards,

Peter

0 Kudos
Reply
6,401 Views
iceice
Contributor III

In SW32R294_RADARAPPDEMO_1_1_0, what are the meanings of TDMIMO and DDMIMO respectively? Is there any relevant documentation

0 Kudos
Reply
6,382 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

The documentation is part of RSDK release.

Please have a look at RSDK user manual for description of TDMIMO and DDMIMO .

c:\NXP\S32R294_RSDK__1_1_0\Docs\

petervlna_0-1661754298693.png

Best regards,

Peter

0 Kudos
Reply
6,363 Views
iceice
Contributor III

      I want to use the cascade mode of S32R294 to connect two TEF8102s. The two TEF8102s operate completely independently, and SPT time-sharing  processes ADC data , Equivalent to replace two S32R274 functions with S32R294;

     But I see the relevant manual of S32R294 says that CSI2 in cascaded mode must be the front end of the master-slave relationship, and only supports TEF82XX; Is my usage feasible?

iceice_0-1661851303389.png

 

0 Kudos
Reply
6,350 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

TEF81xx is capable of cascading. But none of our application boards supports it for TEF81xx.

I am curious about the screenshot, it looks like from RSDK reference manual.

Are you going to write the application yourself or you are going to use RSDK SW? Because RSDK does not support it as it express.

You will need TEF82xx for sure usecase.

Best regards,

Peter

 

0 Kudos
Reply
6,339 Views
iceice
Contributor III

Yes, this is the RSDK reference manual(SWS32R294_RadarSDK_1.4.0_D2207);

I read the code SW32R294_RADARAPPDEMO_1_1_0, which does not seem to support my usage. I need to write some code to support it.

Since I haven't got the development board yet, I would like to confirm whether the scheme of S32R294 and two TEF81XX is feasible

What is the master-slave mode of TEF82XX? Can I use these two modules independently? In addition, is there any documentation related to TEF81xx cascade usage?

Thank you

0 Kudos
Reply
6,333 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Since I haven't got the development board yet, I would like to confirm whether the scheme of S32R294 and two TEF81XX is feasible

This is not supported in HW or the SW. Cascading is supported for Barracuda (TEF82XX) with the CAB.
On top of that you can only connect a single BEST3 TEF81xx to the RADB board.

What is the master-slave mode of TEF82XX?

master - slave is the cascading mode, where one TEF82XX configures the other.

In addition, is there any documentation related to TEF81xx cascade usage?

No, only reference manual.

Best regards,

Peter

 

0 Kudos
Reply
6,313 Views
iceice
Contributor III

Thank you for your answer.

iceice_0-1662347605093.png

 

  What I mean is whether such usage is supported on the chip function. If possible, I will make my own hardware and software

0 Kudos
Reply
6,304 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

As I have said. Cascading is not supported in HW for TEF810x.

This is what I understand from RADAR team explanation.

So for cascading applications please use TEF82xx.

Best regards,

Peter

0 Kudos
Reply
6,300 Views
iceice
Contributor III

I'm sorry, maybe I didn't make myself clear;

My method of use should not be considered as cascade. I use two TEF810X to connect to two CSI2 interfaces of S32R294 respectively.

          They have different configurations and independent operation, for example, one is one with one receiving, the other is three sending and four receiving. SPT processes two pieces of data in time

0 Kudos
Reply
6,272 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Yes, this is possible.

The S32R294 supports connection of 2 front end AFEs.

Best regards,

Peter

0 Kudos
Reply