pn7161 initial firmware

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

pn7161 initial firmware

296件の閲覧回数
user_ahmed
Contributor II

HI

I'm trying to connect pn7161 with esp. 

but I'm failed 

my question is any initial firmware i must burn in begging or dirictly i can connect IC with any another board 

0 件の賞賛
返信
5 返答(返信)

282件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @user_ahmed 

PN7160/1 is a frond-end product, which cannot  work alone, must work together with Host, like MCU. So, you mentioned "esp", is it a type of Host? if so, esp can communicate with PN7161 via I2C or SPI.
Also, you bought the IC, which has default FW, when it worked with the Host, its FW can be updated to the latest version.

0 件の賞賛
返信

280件の閲覧回数
user_ahmed
Contributor II
any library available to communicate between host and ic ?
0 件の賞賛
返信

270件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @user_ahmed 

It's recommended that you can refer to SW6705 - PN7160 NXP-NCI MCUXpresso Example Project, which is based on MCU projects.

Please log in Plug-n-Play NFC Frontend with Integrated Firmware | NXP Semiconductors to download it.

0 件の賞賛
返信

265件の閲覧回数
user_ahmed
Contributor II

PN7161 does not have working firmware in RAM. it tries to upload firmware, but in my setup the firmware file is missing. so i need your help  find/download the correct firmware array from NXP’s package where the basic file in package that i need thanks

0 件の賞賛
返信

247件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信