pn7161 initial firmware

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pn7161 initial firmware

298 Views
user_ahmed
Contributor II

HI

I'm trying to connect pn7161 with esp. 

but I'm failed 

my question is any initial firmware i must burn in begging or dirictly i can connect IC with any another board 

0 Kudos
Reply
5 Replies

284 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @user_ahmed 

PN7160/1 is a frond-end product, which cannot  work alone, must work together with Host, like MCU. So, you mentioned "esp", is it a type of Host? if so, esp can communicate with PN7161 via I2C or SPI.
Also, you bought the IC, which has default FW, when it worked with the Host, its FW can be updated to the latest version.

0 Kudos
Reply

282 Views
user_ahmed
Contributor II
any library available to communicate between host and ic ?
0 Kudos
Reply

272 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @user_ahmed 

It's recommended that you can refer to SW6705 - PN7160 NXP-NCI MCUXpresso Example Project, which is based on MCU projects.

Please log in Plug-n-Play NFC Frontend with Integrated Firmware | NXP Semiconductors to download it.

0 Kudos
Reply

267 Views
user_ahmed
Contributor II

PN7161 does not have working firmware in RAM. it tries to upload firmware, but in my setup the firmware file is missing. so i need your help  find/download the correct firmware array from NXP’s package where the basic file in package that i need thanks

0 Kudos
Reply

249 Views
KaiLi
NXP TechSupport
NXP TechSupport
0 Kudos
Reply