no git access?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

no git access?

1,108件の閲覧回数
tomas_g_fors
Contributor I

Is there a problem with git.freescale.com

I am trying to build fsl-image-minimal for a t4240rdb board, but fetches times out

0 件の賞賛
返信
1 返信

1,066件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Tomas Fors,

I assume that you are using QorIQ SDK 2.0.

SDK 2.0 can be built in your local  PC without networking environment.

 

Please download both  "QorIQ Linux SDK 2.0 SOURCE ISO" and "QorIQ Linux SDK V2.0 PPCE6500 Yocto Cache.iso" 

from Linux® SDK for QorIQ® Processors | NXP , and install them in the same path.

The source ISO includes recipes and source tar balls, the Cache ISO is used to accelerate the building.

Thank,

Yiping

0 件の賞賛
返信