no git access?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

no git access?

1,087 Views
tomas_g_fors
Contributor I

Is there a problem with git.freescale.com

I am trying to build fsl-image-minimal for a t4240rdb board, but fetches times out

0 Kudos
Reply
1 Reply

1,045 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Tomas Fors,

I assume that you are using QorIQ SDK 2.0.

SDK 2.0 can be built in your local  PC without networking environment.

 

Please download both  "QorIQ Linux SDK 2.0 SOURCE ISO" and "QorIQ Linux SDK V2.0 PPCE6500 Yocto Cache.iso" 

from Linux® SDK for QorIQ® Processors | NXP , and install them in the same path.

The source ISO includes recipes and source tar balls, the Cache ISO is used to accelerate the building.

Thank,

Yiping

0 Kudos
Reply