ncp_device example code not working on FRMD-RW612 board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ncp_device example code not working on FRMD-RW612 board

1,343件の閲覧回数
LOKENDERVASHIST
Contributor I

Hello Everyone,

I wanted to run ncp_device example code on FRDM-RW612 board which is not working.

IDE used : MCUXpresso IDE v24.12

SDK used : LOKENDERVASHIST_0-1747890582736.png

When flashed the code on FRMD-RW612 got a hard fault error as shown below:

LOKENDERVASHIST_2-1747890828383.png

 

Can anyone help me with this issue debugging ?

 

 

 

0 件の賞賛
返信
3 返答(返信)

1,285件の閲覧回数
LOKENDERVASHIST
Contributor I

Hello Shaun , 

Please find attached .axf file 

0 件の賞賛
返信

1,101件の閲覧回数
shaun_wu
NXP TechSupport
NXP TechSupport

Hello @LOKENDERVASHIST 

 

Sorry for late reply. It works on my board. Could you try unlock your FRDM board?

Disconnect and connect your board with the ISP button pressed.

 

Best Regards

Shaun

0 件の賞賛
返信

1,297件の閲覧回数
shaun_wu
NXP TechSupport
NXP TechSupport

Hello

 

Could you share built .axf or .bin file to us?

 

Best Regards

Shaun

0 件の賞賛
返信