imx8 Yocto Build throws an error related with m4-native-1.4.17-r0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8 Yocto Build throws an error related with m4-native-1.4.17-r0

1,442 Views
waltersnowwhite
Contributor I

Please see the error log below,

ERROR: m4-native-1.4.17-r0 do_configure: configure failed
ERROR: m4-native-1.4.17-r0 do_configure: Function failed: do_configure (log file is located at /home/builduser/Documents/fsl-arm-yocto-bsp/bld-xwayland/tmp/work/i686-linux/m4-native/1.4.17-r0/temp/log.do_configure.20892)
ERROR: Logfile of failure stored in: /home/builduser/Documents/fsl-arm-yocto-bsp/bld-xwayland/tmp/work/i686-linux/m4-native/1.4.17-r0/temp/log.do_configure.20892

Any help on this is highly appreciated

Tags (2)
0 Kudos
Reply
1 Reply

1,293 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Walter,

DId you start from a fresh build directory? if no, you tmp may be 'poluted' from previous builds. Try cleaning sstate data from that particular pkg. bitbake -c cleansstate pkg

I wasn’t able to find information about this specific error that may help.  You may want to remove the package if it’s not indispensable for the image in question or otherwise try to fix the configuration mismatch, which may be tricky.

Regards

0 Kudos
Reply