SJA1105 Ethernet latency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SJA1105 Ethernet latency

523 Views
stephanernst
Contributor I

I don't find informations in the datasheets of the Automotive Ethernet Switch SJA1105 about Ethernet Latency. I measure about 80us, but is that a realistic number?

Where can I find performance data like this?

I'm interessted in latency with variable packet sizes.

0 Kudos
1 Reply

433 Views
bpe
NXP Employee
NXP Employee


80uS can be realistic or non-realistic, depending on how
you measured it. Strictly speaking, frame latencies are not specified because they depend on
multiple factors. Some discussion of the latencies you should expect can
be found in AH1704, Section 8. The document is available on  Docstore


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos