I am working on an imx6dl-powered custom hardware and I need to implement the HAB, as far as I noticed I have:
- SPL
- u-boot.imx
- kernel fitImage
The build is done using Yocto but the signature is done afterwards using a script I inherited from another project which is able to sign SPL, u-boot.img and kernel fitImage using CST tool, I am trying to use the same script for this project but I am not sure about the signature of u-boot.imx. The script is able to generate the IVT, the CSF, to pad and to concat the signature to the padded binary and so on, but in order to get the u-boot image size (used to computate load address, IVT address, CSF address) it does:
$(od -j 0x04 -N 0x4 --endian=big u-boot-image.bin -t x4 | sed -ne 's/0*04[[:space:]]/0x/p')
which I think is good for fitImages but not really for my u-boot.imx which is a:
dumpimage -l u-boot.imx
Image Type: Freescale IMX Boot Image
Image Ver: 2 (i.MX53/6/7 compatible)
Mode: DCD
Data Size: 61536 Bytes = 60.09 KiB = 0.06 MiB
Load Address: 00907420
Entry Point: 00908000
HAB Blocks: 0x00907400 0x00000000 0x0000cc00
DCD Blocks: 0x00910000 0x0000002c 0x0000000
so, the question is, how to CST-sign a Freescale IMX Boot Image? How to properly generate IVT (which should already be present after Yocto build..) etc?
I also have a u-boot.img which seems to be a u-boot fitImage, but my project requires u-boot.imx
Moreover, yocto provides SPL.log (containing the HAB Blocks) but not a u-boot.log
Thanks in advance!
Hello @Harvey021 and thanks for your reply,
it is very useful actually, but let's say that it would be a little long to integrate the changes into an already existing project...
So let's say that I already have a script coming from older projects which is able to sign:
- SPL (using SPL.log)
- u-boot.img (I assume it's treated as u-boot fitImage since running "dumpimage -l" shows all the contents)
- kernel fitImage
which also generates the CSF and IVT and I need to adapt it to another project which makes use of u-boot.imx (also, in this case, should I care about SPL? Or u-boot.imx will include both!?)
I need a way to figure out if the signed files are OK or not (in terms of signature position and so on) before deploying them on a fused target..
For instance, I can run like:
cst-4.0.0/linux64/bin/hab4_image_verifier ../u-boot.imx.signed <offset>
and, if I use offset=0x0 I have:
File: ../u-boot.imx.signed
Offset: 0x0
Image Vector Table:
Offset: 0x0
IVT Tag: 0xD1
IVT Version: 0
IVT Length: 0x20
HAB Version: 0x40
Entry: 0x908000
DCD: 0x0
Boot Data: 0x907420
Self: 0x907400
CSF: 0x914000
Invalid CSF tag
While if I use 0xd45ec, I get like:
File: ../u-boot.imx.signed
Offset: 0xD45EC
Image Vector Table:
Offset: 0xD45EC
IVT Tag: 0xD1
IVT Version: 0
IVT Length: 0x20
HAB Version: 0x41
Entry: 0x177EDD40
DCD: 0x0
Boot Data: 0x0
Self: 0x177FDD40
CSF: 0x177FDD60
Command Sequence File (CSF):
Offset: 0xD460C
CSF Tag: 0xD4
CSF Length: 80 bytes
HAB Version: 0x41
Command:
Command Tag: 0xBE
Command Length: 12 bytes
Processing 'Install Key' command...
Flags: 0x0
Protocol Tag: 0x3 (SRK certificate format)
Algorithm Tag: 0x17 (SHA-256 algorithm)
SRK Table processed
Source Index: 0
Target Index: 0
Certificate Offset: 0x50
[............]
SRK Table Hash: 23969F270F41....
Key 1:
Offset: 0xD4E9C
Length: 1363 bytes
Invalid key length
Signature 1:
Offset: 0xD53F0
Length: 770 bytes
Invalid signature length
For SPL, 0x0 is correct, in the sense that I have a similar output including the invalid key and invalid signature length
Same thing for the kernel fitImage, with offset 0x0 I don't have any IVT table (since it's not present from yocto) but after signing I can see all the info (including invalid key and signature length) at offset 0x1623000
On another parallel project (which doesn't make use of SPL) we can have a similar output, including the invalid key and invalid signature length using offset =0x0 when checking u-boot.imx
I am currently working with an imx6dl is the "Entry: 0x908000" present in IVT table correct?
Thanks in advance
Best Regards
Renato
Hello, thanks for your answer!
Problem is, my SPL.bin and u-boot.imx have the same IVT table
File: u-boot.imx
Offset: 0x0
Image Vector Table:
Offset: 0x0
IVT Tag: 0xD1
IVT Version: 0
IVT Length: 0x20
HAB Version: 0x40
Entry: 0x908000
DCD: 0x0
Boot Data: 0x907420
Self: 0x907400
CSF: 0x914000
Invalid CSF tag
So I guess that even if I add a signature at the end of the u-boot.imx, the CSF address may be totally wrong