how to start with Evaluation Board for MC33771C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to start with Evaluation Board for MC33771C

Jump to solution
1,476 Views
Biliti_123
Contributor II

Hello All 

I have purchased FRDM33771CSPEVB  ( IC is MC33771C) development board for battery Management system.

I want to do testing of a battery, Please can anyone help me out how to start with this board

I also have S32K144EVB platform board.

Thanks-

Deepak

0 Kudos
Reply
1 Solution
1,448 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

1. Could you please confirm that the hardware is configured as the image below?

diazmarin09_0-1668101510654.png

 

2. Have you download and installed the MC33771C/MC33772C (Battery Cell Controller) Evaluation GUI?

Once installed, please go to Info and click on Help. You will be able to review all the steps to run the demo.

 

diazmarin09_1-1668101540745.png

 

I hope this information helps.

Regards,

David

View solution in original post

4 Replies
1,460 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Deepak,

I hope all is great with you. 

First, I would like to recommend downloading the User Manual (UM11402) from here. Please review the chapter 3.

Do you have the BATT-14CEMULATOR?

The BATT-14CEMULATOR is a 14-cell battery emulator board that provides an intuitive way to change the voltage across any of the 14 cells and four voltage outputs in order to emulate four external NTC. A minimum of 7 cells and a maximum of 14 cells can be monitored.

diazmarin09_0-1668025848291.png

 

Regards,

David

0 Kudos
Reply
1,452 Views
Biliti_123
Contributor II
Hello
Thanks for connecting, I have already this much of information. Could you please help me out -how to connect the board to NXP design studio software and how to start with an example.
0 Kudos
Reply
1,449 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

1. Could you please confirm that the hardware is configured as the image below?

diazmarin09_0-1668101510654.png

 

2. Have you download and installed the MC33771C/MC33772C (Battery Cell Controller) Evaluation GUI?

Once installed, please go to Info and click on Help. You will be able to review all the steps to run the demo.

 

diazmarin09_1-1668101540745.png

 

I hope this information helps.

Regards,

David

1,422 Views
Biliti_123
Contributor II
thank you
0 Kudos
Reply