efficiency - PF8200

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

efficiency - PF8200

1,506件の閲覧回数
Diwakar07
Contributor III

Hi Team,

Efficiency data for all the Buck converters of PF8200 is needed. Kindly help with the curves.

The input voltage is 5V.

Output configurations:

Buck 1&2 (2phase) - 0.8V, 7A

Buck 3 - 0.8V, 0.1A

Buck 4 - 1.8V, 2A

Buck 5 - 1.1V ,1.5A

Buck 6 - 1.2V , 2A

Buck 7 - 3.3V, 1A

 

0 件の賞賛
返信
2 返答(返信)

1,461件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

Your patience is greatly appreciated.

Please review the response from our specialist below:

Please ask customer to download the PMIC GUI in website:

NXP GUI for Automotive PMIC families

And after customer installing the software, he can open that and use PF8200 part.

 

diazmarin09_0-1684172744387.png

 

and then in the Power tab, you can find the information.

I hope this information helps.

Regards,

David

0 件の賞賛
返信

1,492件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Diwakar07, 

I hope all is great with you. Thank you for using the NXP communities.


I want to let you know that I am currently working on your request. As soon as I get a response, I will let you know immediately. 


I will appreciate your patience.


Regards,
David

0 件の賞賛
返信