efficiency - PF8200

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

efficiency - PF8200

1,502 Views
Diwakar07
Contributor III

Hi Team,

Efficiency data for all the Buck converters of PF8200 is needed. Kindly help with the curves.

The input voltage is 5V.

Output configurations:

Buck 1&2 (2phase) - 0.8V, 7A

Buck 3 - 0.8V, 0.1A

Buck 4 - 1.8V, 2A

Buck 5 - 1.1V ,1.5A

Buck 6 - 1.2V , 2A

Buck 7 - 3.3V, 1A

 

0 Kudos
Reply
2 Replies

1,457 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

Your patience is greatly appreciated.

Please review the response from our specialist below:

Please ask customer to download the PMIC GUI in website:

NXP GUI for Automotive PMIC families

And after customer installing the software, he can open that and use PF8200 part.

 

diazmarin09_0-1684172744387.png

 

and then in the Power tab, you can find the information.

I hope this information helps.

Regards,

David

0 Kudos
Reply

1,488 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Diwakar07, 

I hope all is great with you. Thank you for using the NXP communities.


I want to let you know that I am currently working on your request. As soon as I get a response, I will let you know immediately. 


I will appreciate your patience.


Regards,
David

0 Kudos
Reply