eQADC External Trigger using eMIOS - MPC5674F

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eQADC External Trigger using eMIOS - MPC5674F

ソリューションへジャンプ
3,576件の閲覧回数
marjal
Contributor I

Hi,

We are working on eQADC for MPC5674F. the purpose is to trigger the ADC conversion with the Flag of the eMios Channel 23 configured on Modulus Counter mode.

All the ADC configuration is done correctly and when the eMios23 is configured on Output PWM mode the trigger works perfectly and a conversion is made on every set of the eMios23 Flag.

However, once configured on modulus counter mode, the eMios23 Flag does not trigger the ADC conversion anymore.

Is the emios external trigger is considered only if the channel is configured in one of the output modes ?

Else, is there an extra configuration to be made to make the trigger work even in modulus counter mode ?

Thank you in advance.

Marwen.

0 件の賞賛
返信
1 解決策
3,222件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

Yes, only the eMIOS mode which generate output signal (set/clear output flip-flop) can be use as the ADC trigger.

The MC/MCB modes do not generate output signal so cannot trigger the ADC as you have found.

Regards,

Petr

元の投稿で解決策を見る

3 返答(返信)
3,223件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

Yes, only the eMIOS mode which generate output signal (set/clear output flip-flop) can be use as the ADC trigger.

The MC/MCB modes do not generate output signal so cannot trigger the ADC as you have found.

Regards,

Petr

3,222件の閲覧回数
marjal
Contributor I

I thank you !

marwen.

0 件の賞賛
返信
3,222件の閲覧回数
snehakalkhair
Contributor III

Hi ,

Can you please help me with a sample code which shows how we can trigger ADC using eMIOS.

Regards,

Sneha.

0 件の賞賛
返信