eQADC External Trigger using eMIOS - MPC5674F

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

eQADC External Trigger using eMIOS - MPC5674F

跳至解决方案
3,601 次查看
marjal
Contributor I

Hi,

We are working on eQADC for MPC5674F. the purpose is to trigger the ADC conversion with the Flag of the eMios Channel 23 configured on Modulus Counter mode.

All the ADC configuration is done correctly and when the eMios23 is configured on Output PWM mode the trigger works perfectly and a conversion is made on every set of the eMios23 Flag.

However, once configured on modulus counter mode, the eMios23 Flag does not trigger the ADC conversion anymore.

Is the emios external trigger is considered only if the channel is configured in one of the output modes ?

Else, is there an extra configuration to be made to make the trigger work even in modulus counter mode ?

Thank you in advance.

Marwen.

0 项奖励
回复
1 解答
3,247 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

Yes, only the eMIOS mode which generate output signal (set/clear output flip-flop) can be use as the ADC trigger.

The MC/MCB modes do not generate output signal so cannot trigger the ADC as you have found.

Regards,

Petr

在原帖中查看解决方案

3 回复数
3,248 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

Yes, only the eMIOS mode which generate output signal (set/clear output flip-flop) can be use as the ADC trigger.

The MC/MCB modes do not generate output signal so cannot trigger the ADC as you have found.

Regards,

Petr

3,247 次查看
marjal
Contributor I

I thank you !

marwen.

0 项奖励
回复
3,247 次查看
snehakalkhair
Contributor III

Hi ,

Can you please help me with a sample code which shows how we can trigger ADC using eMIOS.

Regards,

Sneha.

0 项奖励
回复