cannot communicate with SC16IS750 over SPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

cannot communicate with SC16IS750 over SPI

Jump to solution
3,008 Views
Nishihashi
Contributor I

Hi.

I am currently trying to communicate with SC16IS750 over SPI.
I checked RESET signal was H-level, and CPU sent SPI mode 0 signal as following:

SPI_waveform.jpg

This is a waveform on reading RXLVL register at the time of release reset.
I expected to receive 0, but the result was different.

I additionaly checked:

  • Direct connection (MISO/MOSI/CLK etc)
  • 3.3V power
  • Reset is released
  • SPI translation rate is 3.125Mbps

Do I have something wrong?

Thanks in advance.

0 Kudos
Reply
1 Solution
2,997 Views
guoweisun
NXP TechSupport
NXP TechSupport

HI

Please see comment:

1: Please refer to hardware schematic.

2:Read the detail SPI specification on datasheet page51 and follow this timing on operate SPI.

 

View solution in original post

0 Kudos
Reply
1 Reply
2,998 Views
guoweisun
NXP TechSupport
NXP TechSupport

HI

Please see comment:

1: Please refer to hardware schematic.

2:Read the detail SPI specification on datasheet page51 and follow this timing on operate SPI.

 

0 Kudos
Reply