Write custom data to flash in LPC55S28

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Write custom data to flash in LPC55S28

1,446件の閲覧回数
Ridzuan
Contributor I

Hi,

Is it possible to write custom data to LPC55S28 flash area and treating it like writing to EEPROM? If yes, is there any sample code that I can refer to?

Thanks,

Ridzuan

0 件の賞賛
返信
1 返信

1,416件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

I'd recommend to check our examples in the SDK. Many make use of the flash area. In addition if you would like to use different commands in the flash to store data, you may refer to the flashiap1 example in the driver_examples folder when importing an SDK example.

nxf51209_0-1601914811026.png

Here you will find an example to write, read and erase blocks in the flash area.

Hope this helps!

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 件の賞賛
返信