Two Master and one slave by using two PCA95111

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Two Master and one slave by using two PCA95111

ソリューションへジャンプ
1,824件の閲覧回数
Aris_Li
Contributor I

Hello team.

I want to use two Master and one slave by using two PCA95111, each with input ports connected to a SMBUS master. The output ports of the two buffers are connected together. By controlling the EN signal, only one buffer is enabled at any time. Can I use it this way?

Two master one slave.png

0 件の賞賛
返信
1 解決策
1,818件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Aris,

yes, you can use the PCA9511 for your configuration.

JozefKozon_0-1646649806278.png

Please note, that is takes time from low to high on the ENABLE pin to the PCA9511 to be ready. Please refer to Figures 16. 17. 18. and to the Table 5. in the PCA9511 datasheet. 

JozefKozon_1-1646650611132.png

 

With Best Regards,

Jozef

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,819件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Aris,

yes, you can use the PCA9511 for your configuration.

JozefKozon_0-1646649806278.png

Please note, that is takes time from low to high on the ENABLE pin to the PCA9511 to be ready. Please refer to Figures 16. 17. 18. and to the Table 5. in the PCA9511 datasheet. 

JozefKozon_1-1646650611132.png

 

With Best Regards,

Jozef

0 件の賞賛
返信
1,809件の閲覧回数
Aris_Li
Contributor I

Hi Jozef,

Thank you very much for your quick response.

0 件の賞賛
返信