Two Master and one slave by using two PCA95111

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Two Master and one slave by using two PCA95111

跳至解决方案
1,835 次查看
Aris_Li
Contributor I

Hello team.

I want to use two Master and one slave by using two PCA95111, each with input ports connected to a SMBUS master. The output ports of the two buffers are connected together. By controlling the EN signal, only one buffer is enabled at any time. Can I use it this way?

Two master one slave.png

0 项奖励
回复
1 解答
1,829 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Aris,

yes, you can use the PCA9511 for your configuration.

JozefKozon_0-1646649806278.png

Please note, that is takes time from low to high on the ENABLE pin to the PCA9511 to be ready. Please refer to Figures 16. 17. 18. and to the Table 5. in the PCA9511 datasheet. 

JozefKozon_1-1646650611132.png

 

With Best Regards,

Jozef

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,830 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Aris,

yes, you can use the PCA9511 for your configuration.

JozefKozon_0-1646649806278.png

Please note, that is takes time from low to high on the ENABLE pin to the PCA9511 to be ready. Please refer to Figures 16. 17. 18. and to the Table 5. in the PCA9511 datasheet. 

JozefKozon_1-1646650611132.png

 

With Best Regards,

Jozef

0 项奖励
回复
1,820 次查看
Aris_Li
Contributor I

Hi Jozef,

Thank you very much for your quick response.

0 项奖励
回复