Two Master and one slave by using two PCA95111

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Two Master and one slave by using two PCA95111

Jump to solution
1,831 Views
Aris_Li
Contributor I

Hello team.

I want to use two Master and one slave by using two PCA95111, each with input ports connected to a SMBUS master. The output ports of the two buffers are connected together. By controlling the EN signal, only one buffer is enabled at any time. Can I use it this way?

Two master one slave.png

0 Kudos
Reply
1 Solution
1,825 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Aris,

yes, you can use the PCA9511 for your configuration.

JozefKozon_0-1646649806278.png

Please note, that is takes time from low to high on the ENABLE pin to the PCA9511 to be ready. Please refer to Figures 16. 17. 18. and to the Table 5. in the PCA9511 datasheet. 

JozefKozon_1-1646650611132.png

 

With Best Regards,

Jozef

View solution in original post

0 Kudos
Reply
2 Replies
1,826 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Aris,

yes, you can use the PCA9511 for your configuration.

JozefKozon_0-1646649806278.png

Please note, that is takes time from low to high on the ENABLE pin to the PCA9511 to be ready. Please refer to Figures 16. 17. 18. and to the Table 5. in the PCA9511 datasheet. 

JozefKozon_1-1646650611132.png

 

With Best Regards,

Jozef

0 Kudos
Reply
1,816 Views
Aris_Li
Contributor I

Hi Jozef,

Thank you very much for your quick response.

0 Kudos
Reply