Trying to use jpegenc with gstreamer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Trying to use jpegenc with gstreamer

5,377件の閲覧回数
ckuecker
Contributor II

Hello,

 

I am working with the i.MX27 PDK unit, and would like to capture images from the camera using gstreamer and jpegenc.

 

When I try to invoke a pipeline with jpegenc in the PDK,  I get the message  "ERROR: pipeline could not be constructed: no element "jpegenc"."

 

I can run the same command on my Ubuntu Linux box with no error.Other gstreamer pipelines work as they should.

 

Any ideas?

 

Chuck Kuecker

 

0 件の賞賛
返信
2 返答(返信)

2,654件の閲覧回数
ckuecker
Contributor II

I ran gst-inspect | grep jpegenc - nothing found. Doing gst-inspect }jpegenc | grep jpeg returns "typefindfunctions::

image/jpeg, jpeg, jpe, jpg"

 

I've got the good, bad, and ugly gstreamer modules installed. What am I missing?

 

Chuck Kuecker

 

0 件の賞賛
返信

2,654件の閲覧回数
ckuecker
Contributor II

I found the problem. In the gst-plugins-good.spec file, the jpeg plugin is disabled. I just removed --disable-jpeg from the ./configure command.

 

It's building now. Need to test it.